Other Parts Discussed in Thread: PMP40514, , , LMV431, TPS23758EVM-080
Hi, I wanted to leave a post in case this situation looked familar.
I have 3 prototype (custom pcb) boards modeled after PMP40514. I changed the voltage divider to the voltage ref to drop Vout from 12v to 5v.
https://www.ti.com/lit/df/tidryo5/tidryo5.pdf
I have 1 working board, and 2 non-working boards.
Do I need to change the feedback resistors/caps just because Vout changed? I don't think so since that only changes the frequency response, but I'm not really trying to change that (but maybe I did since Vout changed?) In any case I'm starting with the PMP40514 values and one board works.
My working TPS23756 outputs 5.0v just fine at no load with 0.4V peak to peak. The output looks fairly smooth .. sinewave like similar to the TPS23756EVM output as far as I can recall.
My non-working boards output a sawtooth waveform 5.0v average, but about 1v peak to peak. As soon as I load the board with nearly anything at all, the sawtooth starts to "dissolve" like someone poured acid on the waveform. Needless to say, follow in boost/buck regulators depending on the 5v input blink on and off. The POE board starts to click and pop (as a boost/buck would do during a short-circuit)
I admit, I'm still trying to learn all the feedback equations for what looks like a type 2 opamp compensator circuit. But the fact that one board is working makes me think that at least part of the circuit is working, but can't respond fast enough to change under load?
In case you've seen something like this before, is there any conceptual thing I should know that would lead me to find the source of error quicker?
So far here's what I've tried:
Checked for any non-soldered pads (seems okay, even added solder to be sure)
Changed all large capacitors, inductors, transformer, diodes, TP23756 chip, voltage ref LMV431AIMFX-NOPB
Conceptually I'm thinking, hey maybe I'm drawing too much power, but 500ma @ 5v is well within reason.
On the way home I remembered that I tripled up on C24 (active flyback clamp capacitor between the two mosfets) on the working board. Could that be the reason my working board survived, but the other two are browning out? I noticed on PMP40514 Schematic tidryo5.pdf that C24 is noted at 6 * 0.1uF -- does it really mean there are 6 caps if they aren't drawn? I don't think so since the TPS23756EVM and the PCB Plot for the PMP40514 don't show more than one cap.
Anyways, if this situation sounds familiar, please let me know. I'm headed back to the office when I wake up to see if I can figure out what I missed.