This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

choosing Thermisitors

Other Parts Discussed in Thread: TMP117, TMP116

Could you help me find the best thermistor for my application? We are doing a quick spin of our clinical-grade patch to assist in the monitoring that is ramping up around the current COVID-19 pandemic. 

The thermistor option you provided (TMP117 & TMP116) is quite expensive and much more accurate than I would need. We are okay with 1% accuracy. You are competing against a 0402 size standard thermistor which is very cost-effective. To make it easy for our engineers we were thinking a 10kohm value thermistor would work fine and analog output is best for us.

Thank you!

  • Lucas,

      Take a look at the TMP6131DEC. First you need to remember that 1% error, at 98.6F is +1 = 99.6F/-1 = 97.6F. When taking a temperature of a person, 1% is to much. you most likely need closer to 0.1%, but that is my thoughts on fever measuring. The TMP6131DEC will need a one time offset correction, but can be as accurate as 0.5%. With a little engineering it could be closer to 0.3%.

      Make sure to look at the design tool for the TMP6131DEC as it will help you a lot.

      The TMP117 is calibrated for you. The cost is usually offset by not having to calibrate.