This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

usage of the boost converter tps61032

Other Parts Discussed in Thread: TPS61032, TPS61030

hi,

i have a lithium battery, with 3,6V nominal output, and can supply current pulses of upto 3A for a 1s,

Need a 5v supply, 190mA average current, 1,5A burst for 10 ms.

Would like to use a tps61032. It states that it can give upto 1A, 5v .. but later in the datasheet, the graph of max current vs input voltage shows the max current to increase with supply voltage.

Hence would this converter : tps61032 be a good choice.

They have multiple Vout pins, do i need to short all of them and use.

Or the multiple pins are used to drive multiple ics and each pin can give that much current?