This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61026: Power Save Mode

Part Number: TPS61026


Dear all,

I would like to ask about power save mode of TPS61026.

If you check the TPS61026 data sheet, you will find the Power Save Mode function as shown below.


How much load does Power Save Mode work in when Power Save Mode is enabled?
(Our customer is trying to operate this device below Iout = 50mA.)

Best Regards,

Y.Ottey

  • Hi Y.Ottey,

    there is no a special loading to enter PSM, it varies with inductor, capacitor, temp and IC process variation, VIN/VOUT ratio.

    this is an old device, please suggest the latest and better performance device to customer if possible.

  • Dear Li 

    Thank you for your reply.

    I would like to ask adding following questions about power save mode.

    1. In the description of power save mode, it is described that the converter operates when the output voltage falls below the lower limit threshold and enters the power save mode in which the output voltage exceeds the upper threshold, but in the case of TPS61026, the above threshold is Is it as follows?
    ・Upper threshold: About 5.02V to 5.04V
    ・Lower threshold: About 4.98V

    2. Is the switching operation stopped when the TPS61026 exceeds the upper threshold of the output voltage and enters the power save mode?

    3. When the TPS61026 is operating in power save mode, does the input current of the TPS61026 (input current to the VBAT pin) change depending on the time the converter is operating?
    (Does the input current increase if the converter is running for a long time?)

    Regards,

    Y.Ottey

  • Hi Y.Ottey,

    1. where did you find the voltage? I didn't have the threshold of the voltage as it is old device.

    2. yes, the switching will stop.

    3. i don't think so, the average current is the same.

  • Dear Li

    Thank you for your reply.

    I would like to adding question.

    When operating in Power Save Mode, it is stated that whether the output voltage does not exceed the upper and lower thresholds determines whether the converter operates.
    Is the internal comparator used to judge whether the output voltage exceeds the upper and lower thresholds? (If the TPS61026 uses another method, please tell me how this device works.)

    Best Regards,

    Y.Ottey

  • Y. Ottey,

    you are correct. there is internal comparator to determine enter and exit PSM. 

  • Dear Li

    Thank for you reply.

    I understand about PSM method.

    I would like to ask adding question.

    1.If the output voltage exceeds the upper threshold in Power Save Mode and the switching operation stops, is it possible to recognize that the current input to TPS61026 is 0A?

    2. When the converter operates in Power Save Mode, should it be recognized that it operates at the normal switching frequency (typ. 600kHz)?

    Regards,

    Y.Ottey

  • Hi Y. Ottey,

    1. the current should be 1uA instead of 0A,

    2. The frequency is 600Khz when the device switching.