This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM265R1: Higher Current Solution

Part Number: TPSM265R1
Other Parts Discussed in Thread: LMZ36002

Dear Team,

I am looking for solution to replace:

https://www.xppower.com/portals/0/pdfs/SF_SRH05.pdf

Not sure do we have higher current module on the roadmap I am not aware of

48V input

5V output

0.5A output

BR

Kevin

  • Hi Kevin,

    Edit: Correction

    Have a look at the LMZ36002. It is a 60V input rated 2A power module that can output 5V. This is the only other alternative that is rated to 60V and can be used for 48V input application.

    Regards,

    Jimmy