Other Parts Discussed in Thread: BQSTUDIO, EV2400
1. Is there a detailed setting procedure for setting the battery balance? Or you can imitate the instructions.
E.g:
a. Balance configuration [CB] = 1
b. Update status = [OE].....
2. We have used high current (500A), and the current scaling is explained in TRM6.7 Current Scaling.
However, we don't know very well. Are there detailed setting steps?
3. The overcurrents for charging and discharging are OCC1, OCC2/OCD1, OCD2. Can OCC1/OCC2 be set the same?
Because we only need to use one. There is "Latch Limit" in OCD Recovery, we don't quite understand how to use it?
4. In Registers. When it is red, it means protection or the function is activated. When it is green, it means that the protection is released or the function is closed.
Can I understand it this way?
In Data Memory->Settings->Protection->Enabled Protections A, there are bit7~bit0, if here OCC1, OCC2 write "1",
Will the status change to red in Registers? What is the relationship between the settings in Data Memory and Registers?
Sorry, there are so many things I don’t understand~
Adam
Best Regards,