Hello,
I am now evaluating tl4242 and I have following questions.
1, present package choice is only WSON (8) but is there any plan to choose smaller package lineup for the future ?
(Can die size of tl4242 meet smaller package ? )
2, I am planning to use tl4242 as “path switch”.by current sense.
In this case, external current is connected to Vref but not reach Vref limit when external current is flowing.
(for example, current setting is 0.2A and if external current value is over 0.2A tltl4242 path is stopped)
I hope to ask internal structure of IC can accept this use or not.
If it also have any concern, could you teach me ?
Best Regards,
K.Sakai