This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62136: Chaging swiching frequency

Part Number: TPS62136


Dear all,

Our customer is evaluating a sample to consider the TPS62361.
Among them, when we confirmed the load characteristics from our customers,
As shown below, when the load was increased, the switching frequency became faster.
Iout=1A→fsw=1.17MHz
Iout=2.6A→fsw=1.25MHz

Although the switching frequency is described as Typ 1MHz in the data sheet, is this the original operation of the device?

*By the way, they are investigating the load characteristics under the following conditions. ‥
Vin=5-6V
Vout=3V

Best Regards,

Y.Ottey