BQ20Z95 IC
I have a battery that 42 cycles and still is in R_DIS. I have cycled it 6 times to see if it will display 1% error. All my batteries display 1% error typically within 3 cycles. This battery was returned from a customer. I have reset it and re-calibrated the voltage and currrent prior to the 6 cycles. It takes a charge and the FCC looks good but never drops below 3% error. You have any ideas?