Other Parts Discussed in Thread: BQ4050
Hi All,
SLUUBU5A suggests the battery has to be in RELAX state in order for the cell balancing to function properly:
"The bq40z50-R3 is required to be in RELAX mode before it can determine if the cells are unbalanced and
how much balancing is required. The bq40z50-R3 enters RELAX mode when:
|Current()|< Quit Current for at least Dsg Relax Time when coming from DISCHARGE mode or Chg
Relax Time when coming from CHARGE mode."
According to the TRM, for balancing to work the GG needs to calculate the balancing time for each cell. Delta Q and Bal Time/mAh are used to produce these times. OCV measurements are required to produce delta Q for each cell. OCV measurements apparently can only be taken during the relax phase, cells need to relax for at least 5 hours to enter this state.
Question: If the application demands long (~10 hr) periods of operation without battery relaxation (battery starts discharging almost immediately after it is charged, then starts charging...), does this mean BQ40Z50 cannot reasonably balance the cells during these times? It seems to me the balancing timers will simply never be updated until the 5 hr relaxation delay with low current expires, but perhaps I missed something.
Thank you in advance,
Vasily