This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Priority ORing for Three power Supply

Other Parts Discussed in Thread: TPS2663

Hi  Team 

We  are  working on one of  project where  we  need  to power  our  sytem from  three  power  source  

Having details  as  below 

PoE  802.3bt Type 3 60W (with 802.3at Type 2 is power consumption is below 25W)
DC 9 to 52 VDC with 3 way PCB terminal (Phoenix like) with connector (+/-/Ground) and latch/screw. 60 W max
Power Delivery Power Delivery 3.0 @ 60W on the Type-C Port (Power Delivery down to 27W when the power consumption is less than 25W)
General Up to 3 power sources connected at the same time.
Using power from one power source at the same time. Redundant power operation.
Under  volatage  and Over  Voltage  protection 
Short  Circuit  Protection , Priority ( PoE , DC  ,PD)

Please  suggest  us  how  we  can  do  priority  ORing for same .