Hi team,
I would like to use BQ24079TEVM to do the charge measurement. My setting is showing as below.
1. R8:ILIM=1k
2. R11:ISET=1k
3. R16:TS=8.66k
4. (JMP5)EN1=low
5. (JMP4)EN2=high
6. (JMP3) CE_bar=low
7. (JMP1) TMR = RES
8. JMP2 TD = low
9. Battery voltage = 3.7V connect to J3
10. J1 = 5V/2.5A
My setting are showing above. I see the D1 and D2 LED is turn on, but there is no charge current going through the battery. Could you help let me know if anything I missed?
Regards,
Roy