Hello TI Team,
We have a requirement to converter the direct 3-phase voltage to DC 12V/2A,
I found many designs which use discrete components for conversion.
Kindly Let us know If TI has any solution for this.
Reply ASAP
Thanks
Manjunath
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
If you rectify the three phase input with a bridge you could use a simple flyback stage to converter to 12V?
What is the range of the three phase AC input?
Regards
Peter
Hi Peter,
3- phase AC voltage is 440V.
Yes I understand,
Please go through this link : https://www.ti.com/lit/ug/tidu817/tidu817.pdf?ts=1594035662884&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FTIDM-3PHMTR-TAMP-ESD
As per the circuit in page 44, which is used to convert 3 phase voltage to 12V/0.5A.
TPS54060 is the converter used.
My circuit requires more than 2A, how to get more current.can I just replace the switching regulator just as you said to increase the current?
Bear with me, I'm new to power electronics and need your support.
Hi Manjunath,
You need something like this but with a higher power capability. The design uses the UCC28700. The datasheet is located here, .
Hi ,
These are single phase 230V to DC converter,
What we are looking is 3-phase line which is directly connected to one IC and gives a DC volt output
Hi Manjunath,
Sorry TI does not have a suitable part for that application.
Regards
Peter