Hi,
Battery Specs
- Cell Chemistry: NiMH
- Series: BK220SCHU
- Nominal Voltage:1.2 V
- Rating Capacity: 2200 mAh
- Charging: -deltaV per cell is 10mV (cell)
- Rapid Charge temperature: 0-60 degree C
- Discharge temperature: 0-75 degree C
- ChemID: 6112 (TI suggested)
- Battery pack configuration: 10S
During charge phase, as When RMFCC is '0' (Not set) in data memory, i expect RemainingCapoacity is not set equal to FullChargeCapacity, and when the valid NegativeDeltaVoltage occurs, the CHG bit has to move from 1 to 0(Bit HIGH to LOW in Flags(). But I'm not seeing the CHG bit is moving from HIGH to LOW and if this happens i can't terminate the charger using our micro. Because I'm using Flag() CHG to terminate our charger.
I attach the data memory (BEFORE: 1Prova 3.1_RMFCC_Disable_scarica e carica.gg and AFTER: 77Prova 3.1_RMFCC_Disable_scarica e carica.gg ) and log file (Prova 3.1_RMFCC_Disable_scarica e carica), Please go through it.
77Prova 3.1_RMFCC_Disable_scarica e carica.gg.csv
1Prova 3.1_RMFCC_Disable_scarica e carica.gg.csv
Prova 3.1_RMFCC_Disable_scarica e carica.log
Thanks in advance!!
Regards,
Reddy