Hi all,
I have a 12V battery and I wish to provide a USB port on the product that allows just charging. It should be able to charge all standard USB devices, including the iPod and iPhone.
The battery isn't huge, so it has to be a switching regulated system for efficiency. It should only use significant power (>200uA) when a USB device is plugged in - whether this is by detecting when a device is plugged or having a very low quiescent current doesn't matter. I've had problems because all the solutions don't appear to be able to 'shutdown' when a device isn't plugged in or they use too much current all of the time.
What solutions do you think are suitable?
Thanks in advance.