I have attached my circuit without the host part and
requirements:
1.Input from adapter:15V/2.4A.
2.battery ratings:11.1/6.4A.
3.Charging at a rate of 12.6V/1.240A(The battery has 6 cells in which it is arranged in series and parallel network to get 3s.Each cell rating is 3.67V/3.1A).
Can you please help if there any changes that is required that needs to be done.