Part Number: TPS65131
Hi BU expert,
my customer (LG display in Korea) is considering to use TPS65131 same in new project.
Before that, They need to simulate temperature of LCD panel based on IC’s temperature data.
Would you help me to get answer on temp simulation data of per below condition ?
if simulation is not possible, Calculated temperature(Tj / TC) is OK.
Condition is below. MP schedule is 1Q next year. IC’s usage is to provide positive/negative to source driver and gamma in Panel.
Case 1) VCC 3.3V, VDDP 6.0V(Out current 50mA), VDDN -6.0V(Out current 50mA)
Case 2) VCC 3.3V, VDDP 6.0V(Out current 320mA), VDDN -6.0V(Out current 320mA)