This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ21061: Is this the right device?

Part Number: BQ21061
Other Parts Discussed in Thread: BQ25101, BQ25120A, BQ25155

Hi team,

i need a single cell Li battery charger that has the following features/specs:

1. LED state of charge output feature.(to show the charge on battery)

2. 125mA charge current

3. USB input (5.5V to 6V max)

can you please help recommend the right device?

Thanks,

Kevin