Other Parts Discussed in Thread: TPS564201
Hello,
I've been working with TPS2513 for new chargers and it does charge but only at 1A each port, checking DP and DM data lines are at 0.7~1.2V each(depending the smartphones tested)...Voltage level is at 5.07V using step-down converter TPS564201. I share schematic. I also have been checking all forum with same questions and it isn't clear what can be the problem, I level up the input voltage also at 5.25 with an external power supply directly to USB connectors and still no change in DP and DM lines to do USB fast charger divider at 2.7V and 2.0V.
I also use a current-limiting power-distribution switch NCP383 dual output.
The tests have been made with several devices: Apple Iphone XR, Apple Ipad 2019, HTC10, Sony XPERIA, Sony M4 Aqua, Huawei Y9s.
Let me know if I'm missing anything or should there be a new device that replaces TPS2513...