This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2373: TPS2373 design issue(12V high current output)

Part Number: TPS2373
Other Parts Discussed in Thread: PMP21103, , UCC2897A,

Hi:

I already follow "www.ti.com/.../PMP21103" design product(poe splitter).

IC:TPS2373+UCC2897A)
Isolation mode/Class8/ DC 12V output
After Sample Run. Poe splitter function not correct.

Although I haved post E2E question.
But UCC2897 FAE suggest this issue re-post E2E ask TPS2373 FAE.

Please reference this E2E question address

e2e.ti.com/.../3399833

About LED issue. Could you have any suggest?

Thanks!

Caspar

  • Hi Caspar,

    From the TPS2388x EVM GUI screenshot, the PD only consumes 3mA which is not a valid MPS to keep the PSE port on. You will need to increase the PD current to >14mA to keep the port on. Thanks. 

    Best regards,

    Penny

  • Hi Penny:


    I already follow your suggested add more loading. But need output more then 12V/0.4A.

    The LED behavior stable(no blinking).But TPS2388x EVM GUI display"PSE output about 6W"

    In addition, I tried to use the TPS2373-4EVM-758 EVB board. But the EVB board is only 1.94W. (LED display is correct)

    What is the difference between these two designs? Could you have any idea for this issue?

    Thanks!

    Caspar 

  • Hi Caspar,

    Please capture port current waveform with your board connecting to TPS23881EVM(use current probe at the cat 5 cable pair 36 and 45 or pair 12 and 78). Please compare the waveform when the load is 6W (when the LED doesn't blink) and light load (when the LED blinks). BTW, did you enable auto MPS function with TPS2373 on your board? Thanks.

    Best regard,

    Penny

  • Hi Penny:


    I will follow your suggested compare the waveform.
    But sorry I'm not so sure about auto-MPS.
    Our circuit follow TPS2373 class-5 circuit design. Why you asked auto MPS function?
    ( Can it effect VCOUT voltage???)
    About our product TPS2373 circit. Please see the below.

    Thanks!
    Caspar

  • Hi Caspar,

    I thought you were seeing the LED on the PSE board blinking.  Am my understanding correct?

    From the schematic, looks like the auto MPS is enabled. 

    The auto MPS function doesn't change the Vout but it provides valid MPS signal to the PSE port to keep it on. Otherwise, the PSE port would be shut off if there'e no valid MPS current on the port. 

    We will need to look at your port current and voltage waveforms. Thanks.

    Best regards,

    Penny

  • Hi Penny:

    Sorry I'm not so sure about MPS function.
    If I disable auto MPS function. Can it will effect any POE function?
    about pair current waveforms. please see the below.
    (I only posted pair 1 & 2 . because other pair the same this status)

    Thanks!

    Caspar

  • Hi Caspar,

    The waveform clearly tells the MPS requirement is not met when the LED blinks. The PD has to hold 16mA current for at least 7ms out of 317ms. Thanks. 

    Best regards,

    Penny

  • Dear Penny:

    Thanks for your information. But this product is "POE splitter".

    Customer can use 12V output power for any application.

    Could you have any suggest about this issue?(add any load circuit on this circuit??)

    Thanks!

    Caspar

  • Hi Caspar,

    Technically, TPS2373 supports auto MPS function which means TPS2373 can generate valid MPS signal to keep the PSE port on. I am not sure why there's no auto MPS signal from your waveforms. I will ask our PD apps engineer to look into this. Thanks.

    Best regards,

    Penny

  • Hi Penny:


    Thanks so much!
    I will waiting for your information.


    Caspar

  • Hello Caspar,

    Can you take a waveform of the voltage across R30?

    Additionally, can you state the differences between your schematic and the PoE reference design, including the front end?

    Also as a side note, I am not the UCC AE, I am the TPS2373 AE :) 

    If this post answers your question, please indicate so by marking this thread as resolved. Thank you.

     

    Regards, 

     

    Michael P.

    Applications Engineer

    Texas Instruments 

  • Hi Michael & Penny:

    I already check my product about TPS2373 circuit. It almost the same as TI Class 5 EVB circuit.

    But I still can double check it again.

    About R30 waveform, please see below

    • 745mW=> LED blink
    • 8W=>LED no blink
    • 80W=>LED no blink

    Thanks!

    Caspar

  • Hello Casper,

    The Automatic Maintain Pulse Signature (MPS) function should be sending this signal when there is light load condition, but it looks like it is not. Can you compare the voltage on this pin to the voltage on the EVM that is working?

    What could be happening is:

    - the board is not built the way the schematic is

    - parts are not populated correctly

    - the IC is damaged 

    If this post answers your question, please indicate so by marking this thread as resolved. Thank you.

     

    Regards, 

     

    Michael P.

    Applications Engineer

    Texas Instruments 

  • Hi Michael :
    Thanks you for your replied. But the direction is very wide.
    It keep difficult to lock in the problem.

    About IC, I already exchange IC between EVB and my product. But the result is the same.
    could you please provide class 5 EVB for test.

    I really no any idea for this issue.

    Thanks!

    Caspar

  • Hello,

    I would start with the components involved with Automatic MPS and the front end. If it is not the IC, and the schematics are exactly the same, then that leads me to believe either something is installed the wrong value, broken, backwards, something is shorted, etc. 

    If this post answers your question, please indicate so by marking this thread as resolved. Thank you.

     

    Regards, 

     

    Michael P.

    Applications Engineer

    Texas Instruments 

  • Hi Michael & Penny:


    Thanks for your support. I already solved the problem.
    This problem will closed.

    Thanks again.

    Caspar