In my application the use of this IC is designed such that the target has both a USB supply and a battery supply
The battery is in the following scenario assumed to be either fully charged or at least within the required voltage level for this IC at any time.
I want to know if the voltage level at the PMID output of this IC exposes a supply voltage glitch / dip when the USB is either connected or disconnected and if so: what is the duration of this glitch/dip
If it may have any impact: the target either has a current draw of 50mA or 200mA depending on the actual momentary target operating state.
The concern of this, is if the USB supply change-over results in a system reset of the target i.e.the MCU, because of the MCU supply interruption, when the main USB supply is interrupted
Thank you