Hello,
I am developing a battery powered product for IoT application and need to choose the right DC/DC boost regulator (3V3). The specifications are provided below.
The biggest problem is that I can't find proper boost converter which is capable of providing 500mA current and also having a good efficiency at low current 5uA. I have already tried WEBENCH Power Designer tool, but didn't have much success.
The board I am developing will be used for periodic data sending to server (using cellular module). The module will consume around 500mA (peak current) when transmission/reception is active. This will happen only for a short time. Around 99,7% of time the module will be in idle mode which will consume just 5uA. The efficiency of DC/DC boost is essential at this low current.
Specifications:
- Vin,min = 2,0V
- Vin,max = 3,2V
- Vout = 3,3V (fixed or adjustable type)
- Iout,min = 5uA, (99,7% of whole time will be in this mode); I need good efficiency here (at least 50% including all Quiescent currents)
- Iout,average = 140mA, (only 0,3% of the whole time); efficiency should be at least 93% (including all Quiescent currents)
- Iout,peak = 500mA, DC/DC should be capable of providing this current only for a short time (e.g. 100ms), efficiency should be around 90% (including all Quiescent currents)
With the help of TI support we have already narrowed down the choice for DC/DC boost to TPS610981 or TPS61021A.
TPS610981 is of course the better choice, because of very low Quiescent Current at Vin and Vout. But, because it is not available in Webench Power Designer I cannot properly calculate efficiency at 5uA current and different voltages. And also, according to datasheet I am not sure if this boost regulator can provide 500mA at Vin=2,0V as I would need. Am I reading those datasheet charts properly?
TPS61021A is preferred choice, because it is cheaper. I am trying to calculate current consumption for 5uA load with the help of Application Report (Calculating and Measuring the No Load Input Current of the Boost Converter). I am having some troubles with understanding regarding used efficiency in that equation. Should I use 13,1% (according to Webench calculation at 2,1V input and 3,3V output, 5uA) or something else?
Could you please help me with the efficiency calculation at 5uA for both regulators. Also, could you confirm if those two regulators are even ok for my specifications and if yes, which one is better. If any better regulator is available, please let me know.
Thanks in advance,
Jure