This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62743: Vout regulation at light load

Part Number: TPS62743
Other Parts Discussed in Thread: TPS62745

Hi!
I use TPS62743 in li-ion battery-powered application. Supply current 12uA in sleep mode and 8mA in active mode. Vout programmed to 3.0V.

Cin 4.7uF Murata GRM188R61E475KE11

Cout 10uF Murata GRM188R61A106KE69

L 2.2uH Murata LQM2MPN2R2MG0

I see that at Iout less than 5 mA device doesn't regulate the output voltage.

Vin=3.8V Vout=3.2V,

Vin=4.0V Vout=3.4V and so on.

I see no pulses on SW pin. I see pulses on SW pin and regulated Vout if input voltage between 3.3 and 3.6V.

If Iout greater than 5mA device works properly.

On screenshots Yellow - Vin, Green - SW

Vin = 3.6V

Vin = 4.0V