Part Number: TPS1663
Hi Team,
We tested TPS16630PWPR and used a 5.6k resistor (1% accuracy)to connect it to the Ilim pin. According to the specification, the current limit should be 18/5.6k= 3.2A. we used electric load with CC mode, and then slowly increase/decrease the load current to test the protection. During the actual test, the data are shown below.
| Vin | Electric load with CC mode, slowly increase load current till protection | Electric load with CC mode, slowly decrease load current till retry | V(IMON), R(IMON=27k ohm) |
| 5V | 4.12A | 3.04A | 2.809V/2.078V |
| 9V | 4.30A | 2.84A | 2.939V/1.945V |
| 12V | 4.30A | 2.85A | 2.933V/1.945V |
| 15V | 3.41A | 2.98A | 2.312V/2.031V |
| 20V | 3.67A | 3.35A | 2.502V/2.291V |
We hope that the current point is relatively stable. For example, if we set the current point at 3.2A, it should be protected if it is higher than 3.2A, and it should be restored if it is lower than 3.2A. There may be errors +-6% as shown in datasheet, but here test with more than ± 20%.
We also tested the voltage on the IMON pin, which is relatively accurate. We want to use the voltage of this pin to give the ADC pin of MCU to detect the current. If it exceeds 2.2V, turn off the current limiting IC.
I hope to ask below two questions
1: Why is the current protection point of the current limiting IC different from that of the rising and falling protection points? Different voltage values? What is the cause? It is better if you could help to explain the working principle of current limiting of this IC.
2: Is the voltage feedback current value of IMON pin accurate? I think the error in the specification is very small. Is it appropriate to use this foot as the judgment of over-current protection?
| Rilim=5.6k ohm, 1% accuracy | Electric load with CC mode, increase load current till protection | Electric load with CC mode, decrease load current till retry | V(IMON), R(IMON=27k ohm) |
| 5V | 4.12A | 3.04A | 2.809V/2.078V |
| 9V | 4.30A | 2.84A | 2.939V/1.945V |
| 12V | 4.30A | 2.85A | 2.933V/1.945V |
| 15V | 3.41A | 2.98A | 2.312V/2.031V |
| 20V | 3.67A | 3.35A | 2.502V/2.291V |