HI Team
Would you advise following two questions,
1, For the "BQ34Z100PWR-G1", will the battery level information be reset if the battery is removed during use
and the fuel gauge IC is not supplied with power, and then the same battery is connected again?
2, If the battery is removed during use and a battery with a different remaining charge(not fully charged)
is connected, what kind of charge will the battery show? ( Represents the previous battery remaining status
OR accurately represents the newly connected battery remaining status OR represents a completely unreliable value
OR other?)
Thanks
Best regards,
Shidara