Other Parts Discussed in Thread: LM5143
Hi Sir:
Is the TPS40170 supports multi-phase function through Master/Slave topology???
if yes, The below connection is right or wrong:
1. Master's M/S pin pull-up 10K to VIN. --> set as Master.
2. Slave's M/S pin direct tied to GND. --> set as Slave.
3. Master's SYNC pin output to Slave SYNC pin through a series resister 4.99K.
4. Both Enable pins connected together by a generator.
5. Both UVLO pins connected together by a divider resistor.
6. Both TRK pins are connected controller owned VDD power.
7. Both SS pins respectively are tied a Capacity to GND. same capacitance.
8. Both RT pins respectively are tied a Resister to GND. same resistance.
9. Both ILIM pins respectively are tied a RC to set over current point.
10. Both FB and COMP pins respectively have feed back resister and RC compensation group.
Thank your help.