Hi,
due to noise reduction and better PSRR as mentioned in the datasheet I want to use feedforward capacitors of 0.01 µF each. As described in chapter 2.3 of https://www.ti.com/lit/an/sbva042/sbva042.pdf I can protect FBP pin against undervoltage.
But how should I do this with the FBN pin? This pin has typically 3.7 mV and can reach 10 mV or down to -10 mV. The Absolute Maximum Rating for FBN is 0.3 V. A schottky diode against GND could compromise feedback loop, I think.
How to protect FBN against overvoltage when negative input voltage and negative output voltage collapse?
Thank you,
Regards,
Marko