Hi team,
- Isn’t pull-up resister needed at ENUV pin if UV function is disable.
Can customer tie ENUV to more than 1.42V such as VIN ? - Can customer tie OVP to GND directly ?
- In soft start operation, inrush current exceeding ILIM will not be seen ?
- Maximum current is the number configured by ILIMIT at startup ?
- In the power down, if the voltage of input pin is dropped first, external protection diode is not needed ?
Thank you and best regards,
Michiaki