Hi all,
I hope everyone is doing well! I was wondering about the margin for safety of using the LM76003 to create an output of 20V at 3.25A when the maximum output current limit is 3.5A. It appears that Webench can successfully simulate the output, but I would like extra reassurance that this output can be achieved in a real world scenario.
Thank you in advance for considering my question and I hope to hear back soon!