Hi all,
I hope you are doing well! I have some confusion concerning the example USB-C application shown below. In this circuit operating at 500kHz, the example uses a 10uH inductor to satisfy the 5V to 20V output range. However, from equation 10 in the datasheet of the LM61460, we find that the minimum inductance needed to avoid subharmonic oscillation would be at least 0.32* VOUT/fSW. With Vout=20V, we find that we would need an inductance of at least 12.8uH to satisfy this requirement. Is the inductor in the example incorrectly used or is this more of a general guideline to follow? How much variation can we have to work around this restriction?