This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC/DC IC request

Other Parts Discussed in Thread: LM5122, LM25037

Dear Sir

Could you help to provide your suggest ,the request as follow :

The Dual input/output DC/DC PSU(160W), Dual Input range is -18Vdc ~ -76Vdc ,Output are 12Vdc (90%) 5Vdc(10%)

The Dual input would independent、simultaneous operation and need Anti-backflow/OVP/OCP/SCP/OPP function.

Could you help to provide the recommended IC ?