This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH05060W: Power Module

Part Number: PTH05060W

Hi,

We are using PTH05060WAH in one of our applications. The unit is fabricated and working fine for the last 8 years. Now environmental specifications are slightly changed. We need a module that has storage temperature of – 55°C. The alternate part number can be with 6A  to 10A rating. Please suggest a drop-in replacement or equivalent module PTH05060WAH .

Madhuri

  • Hi Madhuri,

    Since these are older "plug-in-power" modules, there have not been any upgrade to this specific device that are direct "drop-in replaceable".

    However, perhaps you can look at the PTH04T240W as a starter since it has the following features that are similar to the PTH05060WAH:

    • Up to 10A output current 
    • 2.2V to 5.5V input voltage (low voltage)
    • Auto-Track sequencing
    • Tstg=  -55C to 125C

    Regards,

    Jimmy