This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24616EVM: NO charging

Part Number: BQ24616EVM


Hi 

I just purchase the BQ24616EVM and the unit is not charging and stat light is off. 

* Vin is 20V-24V,

* Battery is 4 cell series 3.7V per cell. Vbat is set for 15.2V

* ACDRV , CE, PG Led is ON.

* No current is drawn from VIN

* It seems the charging is been disable.

* REGN is 6V

* Stat1 and 2 is 1.7V

* ISet1 is 0.599

* ISet2 is 0.299

Please let me know if you need any other data

What could be the issue?

Thank you