Part Number: BQ25790
Other Parts Discussed in Thread: BQSTUDIO
Hi,
There's something in register definition I'm not 100% sure. For example, in REG01 as below we see the fixed offset is 0mV. DOes it mean the battery voltage limit would be 10mV if VREG_10:0 is configured as 00000000001? But, it's also telling us the range is 3000mV min. Does it mean we should not configure this register to any value lower than 00100101100?
Thanks!
Antony