This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50EVM-561: Maximum charge/discharge current limitation

Part Number: BQ40Z50EVM-561
Other Parts Discussed in Thread: BQ40Z50

"Charge and discharge current"    minimum: 0, typical: 2, maximum: 7A

Hi,

Above SS is from the "bq40z50EVM QuickStart Guide". Why is there a limitation on the maximum charge/discharge current (only 7A. 32A is supported on bq40z50, isn't it? Also protection FETs are 11A rated). As I understand, FW setting OCD register can be used to set the overcurrent trip. What is the maximum OCD amperage possible?