Hi team,
we are using the TPS61177A in tablet and met some question in dimming.
DIMMING MODEL: Mix
Frequency:600khz
schemtic:
input: single cell
Load:9x6 LED
Output voltage:27V@21x6mA
question:
when change the D of PWMB from 0 to 50%, the Light intensity could be change from the incearse of D; However when change the D from 50% to 100%, the light could not be change through PWMB.
could you help give me some insights about this question?
BR
Brandon