I am using the CSD95490Q5MC as a smart controller for a buck circuit in a larger power supply. i am trying to obtain useful information from the IOUT pin and am running into issues. my company has access to the full data sheet but without an example waveform or example circuitry its hard to tell exactly what i should be seeing and how to correctly setup the circuit. i have setup the LOUT pin with 250KΩ resistor as my output inductor is 300nH. TLDR; has anyone had success with the IOUT/ current monitorin circuitry and do you have information as to what i should be seeing on the pin itself/