Other Parts Discussed in Thread: BQ76940, BQ78350
Hi
I need some help to understand how to interface gauge IC bq78350-R1A with AFE bq7694003 and MCU. Here MCU is working at 3.3V(typ) and AFE regulator output is at 3.3V while the gauge IC works at a max. voltage of 2.6V and a typical voltage of 2.5V. The problem here is the another line mentioned in the datasheet stating the input and output voltage range of SMBC and SMBD lines as 5.5V.
What I'm not able to get is, during communication when my MCU is working at 3.3V and gauge IC working at 2.5V, what will be the levels for high side and low side. Is there going to be any compatibility issues in detecting the levels or are they just going to be working fine? Please help me understand this.
Thanks