Hello,
I was wondering what the pros and cons are of using an SMT chip-style inductor for the output of the voltage regulator instead of the typical wire-wound power inductor. The 0805 chip-style inductor is way cheaper but I have always associated this style inductor with filtering, not power supply desing. But I am wondering if the power supply spec is low enough, if the chip-style can be used.
Application: Vin = 12V; Vout = 3.3V; Iout(max) = 130mA; Iout(typical) = 80mA
The chip-style 0805 SMT inductor I am looking at is TDK MLZ2012M100WT000
All of the electrical specs are fine for my application but I am not sure if there is some reason these should not be used for SMPS designs. This one is even shielded.
This is the wire-wound inductor I am looking at alternatively (which has higher power properties that are way overkill) TDK VLS252012HBX-100M-1
Thank you!
Ev