Other Parts Discussed in Thread: LM3409HV
I bought a 3409hv evm and I'm changing it to work with a 2.8A Iled and 0.15A detailed. A design somewhat similar to design 3 of the evm,but with slightly higher output current. The issue I now encountered is that in the lm3409hv datasheet (8.3.4) it states that the inductor ripple current should be greater than 24mV/Rsns. A condition which both design 3, and consequently my design, does not meet.
Is design 3 incorrect or is the datasheet incorrect?
Thanks,