This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5164-Q1: Datasheets show the same output resistances even though they are different currents

Part Number: LM5164-Q1
Other Parts Discussed in Thread: LM5163-Q1,

When comparing LM5164-Q1 with LM5163-Q1, there could be an errata since the first is 1000mA but the second is 500mA.

Both datasheets show 0.73 / 0.33 ohm for the output FETs, which doesnt seem likely!