This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23753A: Increasing Converter UVLO

Part Number: TPS23753A

Good day,

I have an application using the TPS23753A.  This particular design included the ability to power the circuit using an auxiliary adapter in "Option 1" mode - in this case an 18-24V auxiliary input.

I need to increase the UVLO voltage of the converter so that it locks out with an input less than ~15V.

I've considered two options to implement this, the first being a second MOSFET in series with the switching FET enabled by a voltage monitoring circuit.  The second, and certainly simpler option is a 6V Zener in series with the TPS23753A VDD1 input.

Does TI have any suggestions for a modified UVLO Converter voltage with the TPS23753A, or could you provide any comments on the two solutions I'm proposing?

Thank You,
Ben