Hi Everyone,
I'm struggling a bit to get going with this design, I know webench can be used, although I want to do the design myself, including the transformer design.
I've been going through the datasheet, although I want to know whether a reference design is available that I can use to work with.
My requirements are :
Vin : 14 ~ 50V
Iout = 12V,3A
I need isolation and hoping for light load efficiency
If any other controllers are available with design guides and that meet these specs I'd really appreciate a link as I have only found the lm5023
Thanks in advance for any help