This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5146-Q1: Output capacitance effect on compensation question

Part Number: LM5146-Q1
Other Parts Discussed in Thread: LM5146

Hi team,

i have a customer using the LM5146-Q1 and is currently leveraging the design calculator tool.

they have a question regarding the circuit compensation calculation. 

they have three 22uF output caps very close to the device for a 5V output, and they also have several 10uF & 22uF caps further down 5V line meant to be input caps for another circuit. should they add these (10uF & 22uF caps) into the LM5146 calculations as well?

how much capacitance degrade when considering the capacitor decoupling radius effect?

Thanks,

Kevin