This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Survey BUCK solution

Other Parts Discussed in Thread: BQ25616, BQ25611D

Hi Team,

I am trying to find a buck solution and spec is shown as below.

  • Input 12V, 1.2A
  • Output CC/CV : 8V/1.15A~1.28A (cell temp <= 50oC) & 0.128A~0.256A (>50oC)
  •  η>90% and feedback loop should have minimum 10dB gain & 45 degree phase margins.

May I learn from you if we have any solution to promote for customers?