Dear Sir,
I have a project need charge Li-ion battery, the Li-ion battery capacity is 2400mAh
I select use BQ24075T to charge it, and my settings are :
1.Fast charge current is 1.5A, the R(ISET)=604 ohm (1.47A).
2. Input current is 1.5A, the R(ILIM)=1K07 ohm (1.495A).
3. EN2=HIGH, EN1=LOW.
But I have some questions :
1. Is it OK about set fast charge 1.625 hours, R(TMR)= 13K ohm?
2. If Input current lower than charge current of set, The charge current will be follow the input current? (OUT pin is no-load situation)
3. Above question 2 condition, the R(TMR) require modify?
Thank you.