This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Configuring TPS2372 as dual-signature PD controller

Part Number: TPS2372-4EVM-006


Hi,

I have a TPS2372-4EVM-006 evaluation module for testing. I would like to know the following information regarding the same.

1) Can the board configured as a PD controller with dual-signature. If yes, what are the settings required for the same.

2) What is the purpose of the J8 jumper on the evaluation board. I can see Class 4 adjacent to both CLSA (J8) and CLSB  (J9)  .

3) Is there a Type3/4 PD controller evaluation board which supports Dual Signature configuration.

Warm Regards,

Sonu Abraham