This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: For TS pin application.

Part Number: BQ25606

Hi Team,

If the TS PIN does not need to be used when the customer’s battery does not have an NTC,
Is TS pin connected to 10K resistor pull high and 10K resistor pull low?
If the battery is not connected, what is the STAT PIN status?

cid:image002.jpg@01D659C8.8F7FFFB0