We are using TPS63700 part for the 5V to -6V generation. We have designed the circuit for max current of 200mA and we have tested for the external resistive load for the max rating. It working fine. When I connect with the actual load of 60mA requirement, It get shutdown and not recovered till I switch off and ON again. When I try to power up my original circuit with external supplies , it hardly takes only 60mA current. By TPS63700 circuit is proved for 250mA supply current. But I am not able to work with original load.
1. Why this chip is going to shutdown mode ?
2. Why it is not recovered or trying to recover when it went to shutdown mode
3. What is the use of COMP pin capacitor ?
4. How can i increase the soft start current .
Please replay at the earliest
Regards
Mariappan
Hardware Design Engineer
044 47414020
mariappan.subramani@datapatterns.co.in