Other Parts Discussed in Thread: TIDA-010015,
Hello,
I am developing 220-48V PSU, using TIDA-010015 as an example. Essentially schematic is the same, with some small changes in feedback circuit and with bigger Q4 (that is temporary solution). In place of Q5, Q7 are IPP110N20NA. I am having some heating issues with MOSFET drivers U7-U8. When PSU is loaded for 300 W (maximum power available should be 500 W), PCB in places, where drivers are placed, is heating up to 105-110 degrees Celsius. The more the load - the more of the heating. This is without any cooling, and this is by far the hottest place on board. I can confirm that it is, indeed, drivers that are heating up, because I see it quite clearly with thermal imaging camera.
I have tried increasing VDD and REG capacitances, lowering input voltage at VDD pin with no luck. Waveforms at VG also seem normal, without any overshoot.
What could be the reason for heating of those drivers?
Regards,
Aleksey